News

Press Release – cULus Listing of Model P25 ESFR
The Model P25 is an Early Suppression Fast Response (ESFR) fire sprinkler with nominal K-factors of 25.2 (360 metric). Now cULus Listed, FM Approved, and CE certified.
The P25 also has a cULus Specific Application Listing for deck heights up to 48′ (14.6 m). Guards and shields are available pre-installed from the factory and the assembly can be installed using the Model W16 wrench.

Press Release – FM Approval of Model MV Nozzles
The Model MV Spray Nozzles are open directional spray nozzles designed for use in water spray fixed systems for fire protection applications. Now cULus Listed and FM Approved.
Press Release – Model FX Dry Pipe Valve
The Model FX Dry Pipe Valve is a differential type, externally resettable valve used to control water flow to a sprinkler system subject to temperatures below 40°F (4°C).
Press Release – Model WP Series Window Protection Sprinklers
The Model WP Series Sprinkler is used with fixed glazed assemblies to create a cULus Listed alternative to a fire-rated wall. The Model WP Series is a 5.6K (80 metric) Fast Response Specific Application Pendent Vertical Sidewall Sprinkler that is Listed to provide complete wetting of various glass surfaces.
Press Release – Sales Personnel Promotions and New Hires
Reliable® is delighted to announce several promotions and new hires for our Sales team: Kyle Claypool-Sales Representative, Daniel De Dominic-Sales Representative, Erin Holleran-Sales Pricing Manager, Rebecca McIntyre, Regional Sales Manager and Clint Williamson, Regional Sales Manager.
Press Release – Locations Update
Reliable® is excited to announce the relocation of its Lorton, Virginia operation to Capitol Heights, Maryland and the opening of a new Distribution Center in Richmond, Virginia.
Press Release – KFR
KFR Series sprinklers are standard spray, quick response sprinklers with a fusible link operating element.
Reliable turns 100!
On January 23rd, 1920, Frank J. Fee incorporated the Reliable Automatic Sprinkler Co., Inc. From our humble New York beginnings to a 21st-century global organization, Reliable is proud to serve the industry with integrity, ingenuity, quality and a commitment to service. We’re excited to begin our Centennial era and look forward to celebrating with you this year.
Follow our Centennial story through the coming year: www.reliablesprinkler.com/100